re:MPC8543 with Memory card interface.   I have a custome...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

re:MPC8543 with Memory card interface.   I have a custome...

Jump to solution
1,563 Views
JimBrosnahan
Contributor I
re:MPC8543 with Memory card interface.
 
I have a customer that wants to include a standard memory card interface on their own MPC8543 board.
Any suggestions on which one might have the easiest interface, example schematics or uboot
drivers?
 
The hardware designer wants to put something on the board now that will be able to hold as much
code as they might eventually have.
 
8543 has no ATA, USB, or SPI
 only local bus, I2C , PCIexpress and DUART
 
Thanks for any help or opinions.
 
BR,
Jim Brosnahan
0 Kudos
Reply
1 Solution
825 Views
genuap
NXP Employee
NXP Employee
Compact Flash. You could use this on the local bus. Look at AN2647

http://www.freescale.com/files/32bit/doc/app_note/AN2647.pdf

View solution in original post

0 Kudos
Reply
1 Reply
826 Views
genuap
NXP Employee
NXP Employee
Compact Flash. You could use this on the local bus. Look at AN2647

http://www.freescale.com/files/32bit/doc/app_note/AN2647.pdf
0 Kudos
Reply