put OM15080-K32W

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

put OM15080-K32W

564件の閲覧回数
aws1995
Contributor I

Hallo,

i try to use JN51xx Device Programmer to understand how to flash file to usb OM15080-K32W Dongle, and for that i have the two questions :

1) how i can build the the example of sdk of k32 , from MCUXpesso IDE, right ?

then shall use the hex file and flash it to the usb Dongle ?

2) second question i have always this problem when i need to connect to the usb-dongle using serial connection , and i saw , must be set the board into the Programing model , how i can do that ? and ther is some clear to this dongle k32 usb ?

aws1995_0-1629376294877.png

,regards

0 件の賞賛
返信
1 返信

544件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi,

 

Hope you are doing well. You need to generate the binary, please refer to section 19.11.1 of the MCUXpresso IDE User Guide.

Can you try with the DK6 Production Flash Programmer (DK6Programmer.exe)? (Path: SDK_K32W061DK6\tools\JN-SW-4407-DK6-Flash-Programmer)

You can follow the instructions of section 1.4 of the DK6 Production Flash Programmer User Guide (Path: SDK_K32W061DK6_doc\docs)

 

Hope this helps. If you have any question let me know.

Best Regards,

Ricardo

0 件の賞賛
返信