pn7150 epc class 1 gen2 protocol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn7150 epc class 1 gen2 protocol

707件の閲覧回数
ziv1
Contributor I

hello NXP 

i am using the pn7150 rfid reader 

i am interested in a heat resistant tags and i found one that follows this protocol:

Protocol EPC Class 1 Gen2
Frequency Range (MHz) 860-960 (global)

does the pn7150 supports this protocol ?

best regards

Ziv

0 件の賞賛
返信
1 返信

702件の閲覧回数
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi, 

well in this case the protocol is not the problem, the problem here is that the PN7150 is a HF reader, it is meant to work in 13.56MHz  so as you can notice the tags you mention are out of the operating frequency  of the reader, simply they wont work together. 

the best would be that you  contact our tag manufacturers if you want to work with NFC they can help you with different tags using our catalog of tags, maybe they have a solution to isolate the tag for high temperatures https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS

BR

 

Jonathan

0 件の賞賛
返信