pn7150 epc class 1 gen2 protocol

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

pn7150 epc class 1 gen2 protocol

543 次查看
ziv1
Contributor I

hello NXP 

i am using the pn7150 rfid reader 

i am interested in a heat resistant tags and i found one that follows this protocol:

Protocol EPC Class 1 Gen2
Frequency Range (MHz) 860-960 (global)

does the pn7150 supports this protocol ?

best regards

Ziv

0 项奖励
1 回复

538 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi, 

well in this case the protocol is not the problem, the problem here is that the PN7150 is a HF reader, it is meant to work in 13.56MHz  so as you can notice the tags you mention are out of the operating frequency  of the reader, simply they wont work together. 

the best would be that you  contact our tag manufacturers if you want to work with NFC they can help you with different tags using our catalog of tags, maybe they have a solution to isolate the tag for high temperatures https://www.nxp.com/products/rfid-nfc/rfid-ecosystem:RFID_ECOSYSTEMS

BR

 

Jonathan

0 项奖励