pn5180, AN11802(rev 1.8) respberry pi 5, NfcrdlibEx1_DiscoveryLoop ... doesn's work

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pn5180, AN11802(rev 1.8) respberry pi 5, NfcrdlibEx1_DiscoveryLoop ... doesn's work

ソリューションへジャンプ
491件の閲覧回数
jekim0109
Contributor II

As per AN11802 rev1.8 instructions, sw369328.zip was applied to raspberry pi 5, but the following error occurs.

 DiscoveryLoop Example:

Line: 133    Error - (0xF181) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h

Line: 142   Error - (0xF181) has occurred in NFCLIB

By any chance, isn't it a KERNEL SPI CFG DIR problem? Or is there a problem with SPI setting?

0 件の賞賛
返信
1 解決策
480件の閲覧回数
jekim0109
Contributor II

I solved it.

Board_PiPn5180.h

 #define PHDRIVER_LINUX_USER_SPI

/*#define PHDRIVER_LINUX_KERNEL_SPI*/

元の投稿で解決策を見る

2 返答(返信)
481件の閲覧回数
jekim0109
Contributor II

I solved it.

Board_PiPn5180.h

 #define PHDRIVER_LINUX_USER_SPI

/*#define PHDRIVER_LINUX_KERNEL_SPI*/

469件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Thanks for your sharing.

0 件の賞賛
返信