local dimming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

local dimming

867件の閲覧回数
zhicheng_tao
Contributor I

寻求车载级别 local dimming LED driver IC ,16 channel 以上(包含)。

0 件の賞賛
返信
1 返信

662件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

I recommend you to take a look at the PCA9955B: https://www.nxp.com/docs/en/data-sheet/PCA9955B.pdf

 

The PCA9955B is an I2C-bus controlled 16-channel constant current LED driver optimized for dimming and blinking 57 mA Red/Green/Blue/Amber (RGBA) LEDs in amusement products. Each LED output has its own 8-bit resolution (256 steps) fixed frequency individual PWM controller that operates at 31.25 kHz with a duty cycle that is adjustable from 0 % to 100 % to allow the LED to be set to a specific brightness value.


Have a great day,
Jose

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信