imxrt1064 SERIAL_WRITE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imxrt1064 SERIAL_WRITE

530件の閲覧回数
Thijs1
Contributor II

 

Try to write some bytes to SRAM_OC (0x20280000)

The Downloader SERIAL_WRITE gives response 0x56787856 0x89232389.

What does that mean?

0 件の賞賛
返信
4 返答(返信)

485件の閲覧回数
Thijs1
Contributor II

Hello Diego,

 

Yes, trying to send commands to the i.MX RT 1064,

Sorry, I am quit new to the i.MX processor, just trying to send some data to its RAM.

(We have a number of LPC based product which we program in production using jtag (SWD) and a serial interface.

  Trying to see whether I can do that for new i.MX RT 1064 products too)

 

I send the following:

 

WRITE_FILE     ADDRESS           FORMAT        DATA COUNT       4 BYTES not used       RESERVED

0x04 0x04   0x20 0x28 0x00 0x00    0x20    0x00 0x00 0x00 0x08    0x00 0x00 0x00 0x00    0x00

 

Than I send 8 bytes (for test)

0x00 0x01 0x02 0x03 0x04 0x05 0x06 0x07

 

Now the i.MX sends back to me

0x56 0x78 0x78 0x56 0x89 0x23 0x23 0x89   (I had hoped for 4x 0x88)

 

If I repeat this simple test under jtag (swd), it works fine and I can read the data back.

 

I am sure I do something wrong, hoped the 89232389 response would give me a clue.

 

Best regards,

      Thijs1

 

0 件の賞賛
返信

481件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Thijs1 

Thank you for your response and for your interest on our MCUs. 

I recall that I have seen this return in the past with another customer, to him the ROM returned this  because : the data size that he gave to the write-file command did not match the actual amount of data that he sent via UART.

I do not have experience interfacing the MCU to that low level without commands. But maybe you can check SDPHOST commands and find easily where the error lies, by decoding them. 

Here I wrote an SDPHOST command example. https://community.nxp.com/t5/i-MX-Processors/Serial-download-detail-process/m-p/1794957/highlight/tr...

Also, please find attached the SDPHost user guide MBOOTSDPHOSTUG.

I hope this could help. 

Diego

 

 

 

 

0 件の賞賛
返信

402件の閲覧回数
Thijs1
Contributor II

Hello diego_charles,

Yes, your response helped. I had an issue with bytes and words.

Thank you

504件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Thijs1 

It seems that you are sending SDPHOST commands to the i.MX RT1064. Is this correct?

If yes, the 0x56787856 means that the MCU is on open life cycle  ( no HAb settings)

diego_charles_0-1717619017731.png

I did not found a reference for the 0x89232389. But could you let me know further about the commands that you are using?

Also you need to be aware that the OC RAM area that you are targeting does not overlap with the area that the ROM bootloader is using. 

diego_charles_1-1717619936289.png

I hope this could help. 

Diego

 

 

0 件の賞賛
返信