iMX27 and SDRAM: LPDDR, SDR and.. not DDR?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX27 and SDRAM: LPDDR, SDR and.. not DDR?

3,231 Views
rd_cet
Contributor I
Looking at MX27 datasheet it looks like there is not support for DDR.

Indeed it would be really useful to be able to use common 2.5V DDR instad of LPDDR.
Can anyone give some advice on how  to interface with DDR? If possible in a reasonable manner..
Thanks
0 Kudos
Reply
5 Replies

932 Views
fabio_estevam
NXP Employee
NXP Employee
Take a look at the MX27 Reference Manual. MX27 does support DDR.
 
I suggest you to look at some of the MX27 development tools schematics for reference.
 
Regards,
 
Fabio Estevam
0 Kudos
Reply

932 Views
rd_cet
Contributor I
Hello.
On both MX27 ADS and PDK schematics there is a LPDDR memory, no schematics with DDR.
From the logic point of view there's not difference between DDR and LPDDR, more or less. But looking at the datasheet (pag. 41) I see
"I/O Supply Voltage, DDR" at 1.8V and I don't know if this can be a problem if connecting 2.5V DDR.

Am I missing anything?

Thank You.


Message Edited by rd@cet on 2009-01-16 10:24 AM
0 Kudos
Reply

932 Views
fslaficionado
Contributor I
The datasheet says that the limit for the DDR pads is 1.8V. So you wouldn't be able to use regular DDR, which is 2.5V. You'll have to use mDDR, at 1.8V.
0 Kudos
Reply

932 Views
rd_cet
Contributor I
Yes, I think it too. I was asking if there is any way (some electrical fix) to do it. But probably there is not any  safe and cost effective fix.
0 Kudos
Reply

932 Views
Wayne84
Contributor I
This processor can only suppport low power DDR which is 1.8V, so you cannot use DDR with 2.5V.
0 Kudos
Reply