I keep on having trouble trying to initialize an NTAG.
It keeps giving a timeout error, HAL,IO-TIMEOUT
RFIDDiscover is 4.9.0.0 running on Windows 10 Version 2004 for x64, connected to NXP Pegoda S
This happens with or without Layer 4 Option checked.
Any help is appreciated.
Hi vincentcoli,
Hope you are doing great, can you confirm that you are following this steps:
after this it should be able to perform a PWD authentication in case the tag is secured if it is not, you can start interacting with it.
BR
Jonathan
Hi @vincentcoli ,
it is possible to use SAM with PEGODA and latest RFIDDiscover, there should not be any issue,
but for NTAG there is no point using a SAM, SAM is intended to perform cryptographic operations, focused for Mifare family, NTAG 424 DNA, ICODE DNA and UCODE DNA. maybe the Ultralight EV1 PWDAuth can help you since UL is similar to some of the NTAG family but before using the SAM you have to unlock it and store the keys inside, all the topics regarding SAM are under NDA and cannot be discussed in this forum.
BR
Jonathan
Jonathan,
Thank you for the clarification regarding the SAM and NTAG! I also use MiFare cards and have a SAM AV3 (or SAM AV2) installed in the Pegoda RD710 with DIP switch 1 set to On with RFIDDiscover v4.9.0.0 NDA version.
I have a SAM AV3 installed in the SAM slot, but did not unlock it and store keys inside. Could this be my problem?
Also since these are NDA topics, are relevant documents to get started (SAM AV in Pegoda) available on the NXP DocStore? I have an account.
Vince
Jonathan,
Thank you for your help! I had partial success.
In the RFIDDiscover “New Profile” menu, I select Contactless Reader “RD71x: NXP Pegoda S CL 0 0” .
But I have a SAM AV3 installed in the Pegoda RD710 with DIP switch 1 set to On.
Can I use the SAM AV3 (or SAM AV2) with the Pegoda and RFIDDiscover v4.9.0.0 NDA version?
Regards,
Vince
Jonathan,
Sorry, I entered this question in my other account. The info is the same as above.
Thank you for your help! I had partial success.
In the RFIDDiscover “New Profile” menu, I select Contactless Reader “RD71x: NXP Pegoda S CL 0 0” .
But I have a SAM AV3 installed in the Pegoda RD710 with DIP switch 1 set to On.
Can I use the SAM AV3 (or SAM AV2) with the Pegoda and RFIDDiscover v4.9.0.0 NDA version?
Regards,
Vince