TJA1041AT/TJA1043 error pin status

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA1041AT/TJA1043 error pin status

643件の閲覧回数
Fu1
Contributor I

Hello NXP support,

I used the CAN transceiver TJA1041AT and TJA1043, and found their error pin status not the same.

When communication with TJA1041, the error was low, is it normal?

When communication with TJA1043, the error was high.

They both can communicate normally.

Please confirm the attched:

Fu1_0-1716972081321.png    

Fu1_1-1716972125385.png

Thank you.

BR Victor

 

0 件の賞賛
返信
5 返答(返信)

534件の閲覧回数
Fu1
Contributor I

Hello Tomas,

I found there are 4 TXD dominant recieved ,the error pin of TJA1041 and TJA1043 is different. the same PCBA and SW, no any bus failure. 

Fu1_0-1717386366759.png   

Fu1_1-1717386383400.png

Could you give some suggestions?

Thank you.

BR Victor

 

0 件の賞賛
返信

614件の閲覧回数
Fu1
Contributor I

Hello Tomas,

 

I am so curious why the TJA1043 can clear the flag but the TJA1041 cannot on  the same PCBA and SW.

 

Thank you.

BR Victor

0 件の賞賛
返信

630件の閲覧回数
Fu1
Contributor I

Hello

Could this be related to software?  I found that the error pin of the same chip was raised on another project.

Thank you.

BR Victor

0 件の賞賛
返信

620件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Victor,

It is indeed likely related to your SW as pins ERR_N or ERR (#8) are in both cases active-low outputs, so a low-level indicates a set flag as described in Table 5 of both datasheets. There should be no difference in the behavior of this pin on these HS-CAN transceivers.

BRs, Tomas

0 件の賞賛
返信

596件の閲覧回数
Fu1
Contributor I
Hello Tomas,



I am so curious why the TJA1043 can clear the flag but the TJA1041 cannot on  the same PCBA and SW.

When the Error pin is low, will there be any problem when I go to communicate?

Thank you.

BR Victor
0 件の賞賛
返信