TJA 1043, Clamp.15 Application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TJA 1043, Clamp.15 Application

598 次查看
omerk
Contributor I

Hello,

I want to use the TJA 1043 in an application with Clamp.15 because it has advanced diagnostic capability
Will I have problems when I use the TJA 1043 in Clamp.15?
Does the CAN transceiver act passively when the power is off?
Does it have a negative effect on the BUS line in the vehicle?

nxp-can-kl15.png

0 项奖励
回复
1 回复

577 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ömer,

If VBAT, VCC, VIO are disconnected, the TJA1043 is in OFF mode (please refer to the AH1014) and the function is OFF & CANH, CANL are high impedance, then.

Due to high impedance of CAN ports, no influence to other ECUs connected to the CAN network.

(In Sleep or Standby, CANH, CANL are biased to GND. So, CANH and CANL pins should have load resistance of Ri; 9k to 28kΩ.)

Best regards,

Tomas