TJA 1043, Clamp.15 Application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TJA 1043, Clamp.15 Application

599件の閲覧回数
omerk
Contributor I

Hello,

I want to use the TJA 1043 in an application with Clamp.15 because it has advanced diagnostic capability
Will I have problems when I use the TJA 1043 in Clamp.15?
Does the CAN transceiver act passively when the power is off?
Does it have a negative effect on the BUS line in the vehicle?

nxp-can-kl15.png

0 件の賞賛
返信
1 返信

578件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ömer,

If VBAT, VCC, VIO are disconnected, the TJA1043 is in OFF mode (please refer to the AH1014) and the function is OFF & CANH, CANL are high impedance, then.

Due to high impedance of CAN ports, no influence to other ECUs connected to the CAN network.

(In Sleep or Standby, CANH, CANL are biased to GND. So, CANH and CANL pins should have load resistance of Ri; 9k to 28kΩ.)

Best regards,

Tomas