TEA2208

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TEA2208

542 Views
Danniel
Contributor I

I wonder if a PTC could be placed between the AC L line and the L pin of the TEA2208, as i found the driver  incorrect  when the voltage at L pin of the TEA2208 was unstable,then the bridge mos and TEA2208 damaged. 

0 Kudos
Reply
3 Replies

529 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Danniel,

Im curious what test / condition made the MOSFET and TEA2208 damaged?

Normally, surge test can destroy the MOSFET and TEA2208 due to overstress of voltage or current:

  • MOV or GDT can be used to  make TEA2208 pins voltage less the limiting values during test.
  • MOSFET could suffer huge current during surge test, MOSFET which can afford big transient current should be used.

Several hundred-ohms to Kilo-ohms resistors could be placed between L/N line to L/R pin of TEA2208 may some help on the surge test, but not verified.

BR, Tomas

0 Kudos
Reply

523 Views
Danniel
Contributor I

Hi, Tomas

Thanks for your reply.

The TEA2208 and bridge MOS damaged just under normal functional test.

As the datasheet indicates ,the driver of the IC based on the voltage of the Land N pin ,so if the voltage at L pin of TEA2208 changes while the PTC value increasing  ,will the drivers  become abnormal?

The schematic diagram is as follows

Danniel_0-1702548199898.png

 

0 Kudos
Reply

490 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Danniel,

The L and R pin sink limited current as datasheet described below, so I do not think this would affect the drive voltage so much  of high side MOSFETs with limited resistors.

Pic.png

For any further support, I would recommend you to reach out our local application engineer Mr. Rong Li.

BR, Tomas

0 Kudos
Reply