我在官网TEA1716T查到的250W用户文档资料里是TEA1713,里面的电路是否把TEA1713换成TEA1716就可以了?
Hi,
I am not sure if I correctly understood your question, but the TEA1713 is pin-to-pin compatible with TEA1716 and is more suitable for applications that do not have severe requirements on burst mode operation and do not require a very low standby power consumption.
Best regards,
Tomas
I'd like to use 1716 to do a 250 W switching power supply.The circuit diagram is made of 1713 which in the NXP website user guide.Can I use this circuit by change nothing except 1713?
Hi,
Yes, you can simply replace the TEA1713 by TEA1716 without any other modifications.
Best regards,
Tomas
Where can i buy LP3925 and QP-3325?
i would be very grateful if you could give me a TEA1713 250 W demo board.