SRK revokation on iMX8X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRK revokation on iMX8X

589 Views
Gandalf-kern
Contributor IV

I have read the following: I don't see a seco command in uboot with iMX8X AHAB:

https://community.nxp.com/t5/i-MX-Processors/i-MX8X-permanently-revoke-a-SRK-key/m-p/1209783

 

1)  In u-boot how do I revoke an SRK key?

2)  Can I have two or more SRK keys up to four keys available at boot?

3) Can I revoke and replace a SRK key before closing with a key other than the four SRK keys? Can I create a new SRK table, reprogram the fuses, and replace the SRK key for example?

Tags (1)
0 Kudos
Reply
1 Reply

573 Views
b36401
NXP Employee
NXP Employee

I answered you in case #00340318 you have created.

0 Kudos
Reply