SPI slaver with DMA on MPC5605 lost frames

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SPI slaver with DMA on MPC5605 lost frames

Jump to solution
1,556 Views
卓儒陈
Contributor II

I have debugged the SPI slaver with DMA successfully. But when I found some question that I let this SPI slaver communicate with a SPI master moudle. I think some frames are lost. I think the reason is SPI slaver fill buffer to SPI Tx FIFO and recieve data from Rx FIFO if DMA controller is idle. But as a SPI slaver, once master send data with clock, slaver must recieve it and send data immediately without any pending. So if MCU is busy on memory operation, at the same time SPI master send some data, then some data frames lost. Am I right, and how to deal with the problem. Please give some code or Detailed description, thank you very much.

0 Kudos
Reply
1 Solution
1,181 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you see datasheet, DSPI characteristic, minimum SCK cycle time is specified as 125/83ns (for MTFE=0/1) what gives me maximum frequency of 8/12MHz.

View solution in original post

0 Kudos
Reply
6 Replies
1,181 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Do you see Transmit FIFO underflow on slave device during this error?

1,181 Views
卓儒陈
Contributor II

I also let moudle delay some time after active cs pin, and change CPOL & CPHA at moudle and master, but it is no use, only slow down sclk is useful.

0 Kudos
Reply
1,181 Views
卓儒陈
Contributor II

Thank for your help.

I check the SR of DSPI, the TFUF and RFOF is not active. So I check my code and find that I start DMA transmission second time, but I havn't waited all DMA done flag for first transmission, so I add the waiting code and it seems not lost frames.

But I want to confirm which memory access priority is higher, dma controller or cpu instruction. If cpu is higher, will spi slaver lost data?

I also find a new problem, and need your help. Mcu as a Spi slaver communicate with moudle as a Spi master.

Moudle send 88 99 AA to MCU, and MCU send AA 99 88 to moudle.

When sclk=6MHz,   MCU receive 88 99 AA,moudle Receive AA 99 88. It's ok.

When sclk=12MHz, MCU receive 88 99 AA, but moudle recceive D5 CC C4. It seems that the highest bit is lost in high sclk. I also check the slaver Tx fifo is filled rightly(AA) before receive master's sclk.

I don't find the reason. Each SPI wire(SCLK CS MOSI MISO) length is about 10mm, MCU is MPC5605 its clock is PLL 8MHz to 64MHz. Please help me, thank you.

0 Kudos
Reply
1,181 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

XBAR priority for eDMA master must be set for higher value than the core, it is basically mandatory for such applications. However this device have set fixed XBAR priorities the way eDMA has higher priority then the Core, so it is right.


According to your description I am not sure if you trigger DMA channel proper way. It is needed to use DMA source related to DSPI (DSPI_n_TX or DSPI_n_RX thus source 1-12) for proper command filling and result draining.


It is quite high frequency to drive over piece of wire. You may try to change slew rate control (SIU_PCRx[SRC]) to 1 (medium/fast).

0 Kudos
Reply
1,181 Views
卓儒陈
Contributor II

tek00014.pngtek00012.png

I also send SPI frames without same, it lost bit too. Then I observe the SPI wave on oscilloscope, SPI CPHA=0(data change on SCK's down edge), but I see there is 50ns delay between sclk down edge and data change edge. So after I caculate, I think I can only use SPI slaver with lower than 10MHz sclk. I have already changed slew rate to fast. It seems a trouble.

0 Kudos
Reply
1,182 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

If you see datasheet, DSPI characteristic, minimum SCK cycle time is specified as 125/83ns (for MTFE=0/1) what gives me maximum frequency of 8/12MHz.

0 Kudos
Reply