SJA1124 SPI to Quad-LIN Bridge and Rpi

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SJA1124 SPI to Quad-LIN Bridge and Rpi

768件の閲覧回数
Khaled_tn
Contributor II

Hello, I ordered the SJA1124 EVAL board to try to use it with my raspberry pi. My goal is to succeed in adding the SJA1124 in a hat board for may Rpi and to communicate with it as a LIN device. Any ideas on the requirements to realise this ?  (Drivers, overlay...)
Thank you.

ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

747件の閲覧回数
Khaled_tn
Contributor II

Thank you Tomas, I also found an "SJA1124 - Example software package" in the product webpage and I requested the download permission but I didn't got an answer yet so hope they will accept it

0 件の賞賛
返信

757件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Khaled,

I have not tried interfacing the SJA1124EVB with Raspberry Pi yet, unfortunately.

I would recommend to take a look at our SJA1124EVB Quick Start Guide which illustrates interfacing with our S32K144EVB MCU board. We do also offer an example application which shows usage of the SJA1124 software driver on the S32K144EVB. In the main loop LIN frame is sent on all four of the device channels one after another, waiting for active interrupt pin and set transfer complete flag between transfers. In order to get the example application, a standard support ticket must be created.

BR, Tomas