SBC Failure during Vibration Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SBC Failure during Vibration Test

259 Views
SamikshaKB
Contributor I

Hello,

During one of the endurance tests, failure of SBC IC: MC33FS6523CAE has been observed. 

The resistance between Vpre pin and ground pin of SBC has almost become like short showing impedance of around 40 ohms.

What could have caused such a failure mode? 

0 Kudos
Reply
1 Reply

243 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Samiksha,

Your vibration test might have caused micro-cracks in the solder joints which can create intermittent connections or short circuits. Or it could have caused delamination or damage to the PCB traces, leading to shorts or reduced impedance between pins. The vibration might have caused internal damage to the IC die or bond wires, resulting in an internal short circuit between the Vpre pin and ground.

To diagnose the root cause of the failure, I would recommend to consider the following steps:

1. Visual Inspection: Examine the PCB and the IC under a microscope for any visible signs of physical damage, cracked solder joints or damaged traces

2. X-Ray Inspection: Use X-ray imaging to inspect for internal damage within the IC or to check for solder joint integrity.

3. Reflow Soldering: If solder joint cracking is suspected, consider reflow soldering the IC to see if the issue is resolved.

BRs, Tomas

 

0 Kudos
Reply