S32R41 RSDK GMAC0 ethernet communication(M7-0&&A53)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R41 RSDK GMAC0 ethernet communication(M7-0&&A53)

428 Views
WenChao
Contributor II

I want to use GMAC0 on M7. GMAC0 communication on M7 in the Debug mode of the S32 Debug emulator is also working properly. However, after burning the M7 program into the boot, it was found that M7's GMAC0 communication would be affected by the compilation of the refInit() function in the A53 program, in two cases:

(1) Without adding rfeInit() function, SRAM used more than 600 KB when compiling, and M7 network port communication was normal when the board was powered on;

(2) Add rfeInit() function when compiling SRAM used more than 3500 KB, the board is powered on M7 network port communication to send a frame of data is not sent.

The second RF initialization function( refInit() ) after power-on has not yet been executed,the difference between (1) and (2) is that the GMAC0 network port of M7 will not communicate with each other after refInit() is compiled。

Why is that?

0 Kudos
Reply
2 Replies

404 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Could you please rise a question via NXP.com support?

That way I can escalate it to the RADAR team.

Best regards,

Peter

0 Kudos
Reply

335 Views
yuran
Contributor II

How to rise a question via NXP.com support,Can you give a link ,plz

0 Kudos
Reply