RTC time changing to default values after some time

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC time changing to default values after some time

1,688 Views
pnaven03
Contributor I

Hi Team,

Am using raspberry pi  board , interface with RTC , setting the hardware clock using "hwclock --set" command , reading the clock using hwclock -r command, initially reading properly as a set time but after some time changing to default time values..

Thanks in advance,

Nv.

0 Kudos
Reply
3 Replies

1,464 Views
david_diaz
NXP Employee
NXP Employee

Hello Naveen,

What RTC device are you using? I can help you with its configuration. Can you share your schematic?

Regards,

David

0 Kudos
Reply

1,464 Views
pnaven03
Contributor I

Hi David,

We are using rtc-pcf8563 device and driver registered successfully ,

Initially clock , date setting and reading properly ,

after one day time changed to one hour delay , There is kernel logs for

debug. Please can you help me.

Please check once attachment.

Regards,

Naveen Kumar,

0 Kudos
Reply

1,464 Views
vinodmaverickr0
Contributor IV

Hi Naveen,


This is nxp community. So I think you should ask this question in raspberry community (for better support). BTW you can also get the assistance here if you will elaborate your question (like which RTC module are you using  and if it is on the I2C so you can check the i2c communication through i2c utility) in a precise way.

Thanks,

Vinod

0 Kudos
Reply