PN7160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7160

2,632 Views
Dhvani
Contributor I

Hello,

I am using the NXP PN7160 NFC module on my custom board. In my design, there are no GPIO pins assigned to the DWL_REQ pin on the PN7160. As a result, I am encountering errors when running the 'nfcDemoApp poll' Application.


1) Is it necessary to connect DWL_REQ pin to processor gpio? or

2) What else can I do to resolve this issue?

Thanks in Advance

0 Kudos
Reply
2 Replies

2,619 Views
Dhvani
Contributor I

Hi there, 
Here attaching the log file for the output of nfcDemoApp.

Thanks

0 Kudos
Reply

2,608 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help us check chapter 7.3 Download mode control (DWL_REQ Pin) in the PN7160 hardware design guide

 

Regards,

0 Kudos
Reply