PN5190 VBAT & VBAT_PWR Pin Pad Supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PN5190 VBAT & VBAT_PWR Pin Pad Supply

489件の閲覧回数
Clownfish_xl
Contributor I

PN5190  datasheet describes the supply voltage range

Clownfish_xl_0-1677479552049.png

Clownfish_xl_1-1677479598270.png

Clownfish_xl_2-1677479617353.png

1.When VBAT and VBAT_PWR pins of our PN5190 chip are connected to lithium battery for direct power supply, after EMVco_L1_3.1 certification, the field strength test of NFC will attenuate with the decrease of lithium battery power, so that the field strength test of NFC cannot pass. I would like to ask whether stable 3.3V power supply is recommended for these two pins of PN5190 chip or lithium battery power supply (lithium battery voltage range 3.7V ~ 4.4V) can be used directly. If so, what are the advantages and disadvantages of lithium battery power supply and stable single power supply?

2.The test now uses NXP NFC Cockpit tools for the opening test to ensure that the core NFC field intensity is maximum at 4cm, and the chip temperature is between 70℃ and 85℃. Is this working temperature reasonable? Will the chip temperature increase affect the temperature drift of the components of the NFC impedance matching circuit, thus attenuating the field strength of the NFC?

 

 

 

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)