Hello,
I want to know Is it PN5180 satisfactory with EMV and ISO at the same time?
As I know EMV has to satisfy distance 4cm.
However, ISO has to satisfying distance more than 5cm.
How can I satisfying two conition?
Just using PN5180, Can I do this? Or I have to more something to this?
Please let me know details.
Thanks.
Hello @HoYeongJang
Sure, of course you can. First, the PN5180 is working on ISO/IEC 14443 before it is EMVCO compliant.
First of all, you have PN5180 working following the ISO/IEC14443 protocol standard.
Secondly, the EMVCO feature is implemented under the above conditions.
You can refer to SW352236, which contains routines on how to implement EMVCO.
BR
kelly