PCF85063A RTC - Minute ISR Sticks Low

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF85063A RTC - Minute ISR Sticks Low

395件の閲覧回数
nxf48158
NXP Employee
NXP Employee

I have a PCF85063A in a design, it's the only thing on the I2C bus.

I set the "minute interrupt" by setting bit 5 in control register 0x01.

When this interrupt fires, the INT pin goes low as expected, but it never recovers HIGH unless I send a RESET command (or cycle power).

The pullup resistor is 4.75k, 5V supply.

If I do NOT enable the minute interrupt, the pin never pulls low, as expected.

I am looking for a solution for the INT pin latching LOW when it fires the first time.

Thanks in advance.

0 件の賞賛
返信
1 返信

388件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

I will connect with you in teams later.

0 件の賞賛
返信