PCA9745B SDO stays low

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9745B SDO stays low

18,197 Views
bmerrill
Contributor I

PCA9745B SDO stays in a low impedance state. It does not matter if CS is high or low.

setup:

Reset tied high, OE tied low, VDD supplied with 3.3v. 3.3v logic on SPI

The PCA9745 has been verified to pull the SDO low. when disconnecting the 50ohm resistor to it, the line is no longer held low

0 Kudos
Reply
7 Replies

17,815 Views
kounotetsu
Contributor I

Hi, do you have any resolution on this issue?
I have the same symptom with all of the products.
Although the product functionality is fine, I have never read registers inside, since SDO signal must be disconnected.
I have found same topic in this forum "PCA9745B SDO high-impedance state" which is not solved, too.
https://community.nxp.com/t5/Other-NXP-Products/PCA9745B-SDO-high-impedance-state/m-p/994889

0 Kudos
Reply

18,145 Views
guoweisun
NXP TechSupport
NXP TechSupport

what's the result if disconnect the SDO pin of PCA9745 with MCU side?you can test it!

0 Kudos
Reply

18,146 Views
guoweisun
NXP TechSupport
NXP TechSupport

If you disconnect SDO pin to MCU then test it, what's the result?

0 Kudos
Reply

18,098 Views
bmerrill
Contributor I

The PCA9745B has been isolated from other components on a separate proto-board.

With no connection to the MCU (or anything but a scope), the SDO line still stays low, with Chip select low or high.

Only when in the reset state does the SDO line go high.

3 separate PCA9745B's have been tested and exhibit the same failure type

0 Kudos
Reply

18,173 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you mean your PCA9745B no work normally because of SDO always LOW?

0 Kudos
Reply

18,154 Views
bmerrill
Contributor I

Yes, the PCA9745B is not working normally, as it should go into tristate, or high impedance when Chipselect goes high. Instead, SDO is always low.

0 Kudos
Reply

18,076 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please according and setting your SPI communication timing as datasheet page39-Fig 19. Definition of timing then to try again.

 

0 Kudos
Reply