P3S0200可以工作在1.8V的IIC上吗

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

P3S0200可以工作在1.8V的IIC上吗

267 次查看
赵中飞
Contributor I

P3S0200的VCC我用3.3V,IIC我用1.8V可以吗

0 项奖励
回复
1 回复

258 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Zhao,

please refer to the Table 7. in the P3S0200 datasheet. The VCC voltage sets the VIH and VIL levels for the input pins. If VCC=3.3V, than minimum voltage required on the input pins, to be recognized as logic high it 0.46*VCC=0.46*3.3V=1.518V. You can use the 1.8V for the input pins. The 1.8V will be recognized as logic high.

JozefKozon_0-1700481975929.png

 

With Best Regards,

Jozef

0 项奖励
回复