OM13082 LCD12864 backlight

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OM13082 LCD12864 backlight

1,006 次查看
john_schooling
Contributor I

OM13082 (https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/lpcxpresso-boards/...)

has an LCD12864.

I can't believe there is no backlight.  Have I missed something?

标签 (1)
标记 (2)
0 项奖励
回复
3 回复数

880 次查看
john_schooling
Contributor I

Hi XiangJun,

The pins in your document do not match the display ribbon or the circuit diagram on the OM13082 board.

There is no evidence of LEDA/LEDK on the OM13082 board connector.  There are 20 pins on the LCD and 28 pins on the external end of the ribbon cable.  The unused 8 pins are connected to capacitors on the OM13082 board (presumably for a different LCD display).

Here are the pins:

LCD12864 ribbon FPC-WKG12864...
ST7565S controller
                                      OM13082      OM13082
LCD side    external connector        connector    CCT
========    =======================   =========    =======
 1  CS        1                       CS           R8  -> CS
 2  /RES      2                       RST                 nRST
 3  CD        3                       C/D          R11 -> CD
 4            4                       WR   (NC)    
 5            5                       RD   (NC)    
 6  D0        6                       D0   (NC)    
 7  D1        7                       D1   (NC)    
 8  D2        8                       D2   (NC)    
 9  D3        9                       D3   (NC)    
10  D4       10                       D4   (NC)    
11  D5       11                       D5   (NC)    
12  D6(SCL)  12                       D6/SCK       SCLK
13  D7(SI)   13 1 - 13 = thin wires   D7/SID       MOSI
14  VSS      14 Thick wire            VSS          GND
17  VOUT     15                       VOUT         C20 -> GND
             16 NC                    CAP3P        C14
             17 NC                    CAP1N        C14/C18
             18 NC                    CAP1P        C18
15           19                       CAP2P        C19
16           20                       CAP2N        C19
             21 NC                    V4           C13 -> VDD
             22 NC                    V3           C12 -> VDD
             23 NC                    V2           C11 -> VDD
             24 NC                    V1           C10 -> VDD
             25 NC                    V0           C9  -> VDD
18  C86      26                       L:C86/H:C68  VDD        MPU interface.  H = 6800 series.  L = 8080.
19  P/S      27                       L:S/H:P      GND        L = serial (SCL/SI)
20           28 Thick wire VDD        VDD          VDD
Thanks.
John.
0 项奖励
回复

880 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, John,

Thanks, I see.

BR

Xiangjun Rong

0 项奖励
回复

880 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, John,

The OM13082 board uses LCD12864 as liquid screen, the LCD12864 liquid screen has the backlight pins exactly. The Pin 19 is LEDA pin(it should connect +5V of backlight) , the pin 20 is LEDK pin(it should connect to GND, the GND of back light).

This is the data sheet of LCD12864, but it is written with Chinese.

http://www.dfrobot.com.cn/image/data/FIT0021/CN/LCD12864%20chinese%20char.pdf 

Regarding the board, I think the LEDA/LEDK should be connected to +5V rather than a capacitor.

BR

XiangJun Rong

0 项奖励
回复