I would like to interface between a memory card operating at 1.8 V or 3.0 V signal levels and a host operating at 3.3 V signaling levels.
In Table 7 (Absolute Maximum Ratings), max VCCA is given as +4.6V and max VI as +4.6V.
In Table 8 (Recomended Operating Conditions), max VCCA is given as +2.0V and max VI as VCCA+0.3V (not to exceed +3.6V)
My interpretation is that this part will work for +3.3V LVTTL host-side signaling. Am I wrong?
Hi Erik,
According to the Table 8, the host side interface signal voltage max is 2.3V to guarantee normal operation .
You can try higher voltage up to 3.3V, but the clock rate will drop to 25MHz possible.
Best regards,
Tomas