What is the physical meaning of the T port between the D port and the S port in the ADS model? How to connect in the actual simulation? I saw someone saying that the T port is directly connected to the ground, but some people have set the T port to a value of 25.
What is the best way to use the T pin?
−Load this thermal, T, pin with a large-value resistor.
−The voltage measured at this thermal pin is the temperature rise above the heat sink, TSNK, temperature value in Celsius.
What is the best way to look at memory effects due to thermal changes?
−During a simulation, monitor the voltage at the thermal node.
Have a great day,
Pavel
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------