MSC8156ADS I2CBoot demo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSC8156ADS I2CBoot demo

Jump to solution
1,691 Views
Jim95
Contributor III

Hello, I try to boot on I2C EEPROM, using the I2CBoot demo, but after creatin the .txt and burn it into the EEPROM, when I power off and power on the board it doesn't boot on the loaded program. I followed all the instruction of the text file: file How to.doc. I don't understand why it doesn't work.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
1,052 Views
Jim95
Contributor III
I have find the solution, the addresses of __ctr0_start was not good in the SC3850.mmp file. Now it works fine. Thank You.

View solution in original post

0 Kudos
Reply
2 Replies
1,052 Views
AndrewinApps
Contributor IV

Which version of CodeWarrior are you running?

Regards, -Andrew

0 Kudos
Reply
1,053 Views
Jim95
Contributor III
I have find the solution, the addresses of __ctr0_start was not good in the SC3850.mmp file. Now it works fine. Thank You.
0 Kudos
Reply