MRF6V2150 PA design

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MRF6V2150 PA design

1,014件の閲覧回数
ajivs
Contributor I

Is there matching PA design available for MRF6V2150?

0 件の賞賛
返信
1 返信

885件の閲覧回数
LPP
NXP Employee
NXP Employee

We have no specific application notes for MRF6V2150. The following documents can be useful:

RF Power Device Impedances:Practical Considerations
http://cache.nxp.com/docs/en/application-note/AN1526.pdf

Impedance Matching Networks Applied to RF Power Transistors
http://cache.nxp.com/docs/en/application-note/AN721.pdf

Three Balun Designs for Push-Pull Amplifiers
http://cache.nxp.com/docs/en/application-note/AN1034.pdf

NXP provides reference circuits as they are described in the MRF6V2150 datasheet. You can order these circuits via our distributors. Also, you can request DXF files for these boards from our technical support.
http://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu


Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信