MRF6V2150 PA design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF6V2150 PA design

1,010 Views
ajivs
Contributor I

Is there matching PA design available for MRF6V2150?

0 Kudos
Reply
1 Reply

881 Views
LPP
NXP Employee
NXP Employee

We have no specific application notes for MRF6V2150. The following documents can be useful:

RF Power Device Impedances:Practical Considerations
http://cache.nxp.com/docs/en/application-note/AN1526.pdf

Impedance Matching Networks Applied to RF Power Transistors
http://cache.nxp.com/docs/en/application-note/AN721.pdf

Three Balun Designs for Push-Pull Amplifiers
http://cache.nxp.com/docs/en/application-note/AN1034.pdf

NXP provides reference circuits as they are described in the MRF6V2150 datasheet. You can order these circuits via our distributors. Also, you can request DXF files for these boards from our technical support.
http://www.nxp.com/support/support:SUPPORTHOME?tid=sbmenu


Have a great day,
Pavel
NXP TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply