MMPF0100F6ANES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100F6ANES

787 Views
RamakrishnaC
Contributor III

HI Team,

MMPF0100F6ANES, In this part i am not using the VIN1, VIN2, SW2 and SW4. as per NXP reference document  need connect >3.4V to VIN1 & VIN2 without using the outputs. So shall i connect VGEN6 output(3V) to VIN1 & VIN2?

Please confirm.

Thanks.

0 Kudos
Reply
5 Replies

750 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

I hope all is great with you. Thank you for using the NXP communities.

Correct. Based on the document attached, if VIN1 and VIN2 are not used, they must be connected to the output of a regulator with voltage <3.4V and <3.6V respectively.

I hope this information helps.

Regards,

David

0 Kudos
Reply

734 Views
RamakrishnaC
Contributor III

Hi David,

Thank you.

My queation is shall i connecet the other voltage regulator output to VIN1 & VIN2?

Please review and check my scheamtic complete PMIC configuration and share your feedback details.

Thank you.

0 Kudos
Reply

720 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

Once again, thank you for using the NXP community.

Correct, as long as the output of a regulator is <3.4V and <3.6V respectively.

diazmarin09_0-1719504371438.png

 

Your schematic seems correct to me.

Regards,

David

0 Kudos
Reply

718 Views
RamakrishnaC
Contributor III

Hi David,

Thank you.

And one more conformation needed. 

Can i connect the VGEN6 output voltage to VIN1 & VIN2?

Please confirm.

0 Kudos
Reply

715 Views
diazmarin09
NXP TechSupport
NXP TechSupport

Hello RamakrishnaC,

Yes, you can. As long as VIN3 is supplied, you can connect the VGEN6 output to VIN1 and VIN2.

diazmarin09_0-1719512885576.png

 

I hope this information helps.

Regards,

David

0 Kudos
Reply