According to the spec process, our design is as follows,premise:
Vsup = 24V(always connect the battery) wake1:control by mcu,the MCU detects whether a key is inserted to determine wake1 status. wake2:control by external buttons
Plan on:
In normal state , the MCU detects that the key is not conneted:Set GoTo_STBY =1;Wake1 = 0;
The State change to Standby.
Plan on:
In Standby state , the MCU can't work ,the external button is pressed:
The State change to normal.
In Standby state , the MCU can't work , the external button is not pressed(set Wake2=0):
The State change to Powerdown.
Plan on:
In Powerdown state, hold down the external button of more than 300ms
The State change to standby ,beacse of hold down the external button ,so the state change to normal.
解決済! 解決策の投稿を見る。
Dear 婧芳 郑,
As long as the SBC is normal ,PROB_MAIN =1. It is right?Are my predicted state transition conditions correct?
[A] Yes, that is correct. But do not also forget about the PORB_FS=1 referring to the Fail Safe.
With Best Regards,
Jozef
Dear 婧芳 郑,
thank you for the description. Do you have a question?
With Best Regards,
Jozef
I wonder if my design is up to specification,beacuse now in the design phase.
How do I get the PROB_MAIN status?
Dear 婧芳 郑,
for the PORB status please refer to the section 32.9.1 in the FS84-85 datasheet.
With Best Regards,
Jozef
To MCU PORB is currently designed for I/O connceted to mcu.
Whether PGOOD is equal to PORB_MAIN?
PGOOD low level in standby and power down,but power down need PORB_MAIN = 1,it looks a little strange.
Dear 婧芳 郑,
please see below a question from another customer and an answer from an application engineer regarding the PORB.
DESCRIPTION
Q2. What is the PORB_MAIN as well as PORB_FS referred to in the functional state diagram?
A2: The PORB_MAIN=1 or PORB_FS=1 means the Main logic or FS logic is ok.
With Best Regards,
Jozef
As long as the SBC is normal ,PROB_MAIN =1. It is right?Are my predicted state transition conditions correct?
Dear 婧芳 郑,
As long as the SBC is normal ,PROB_MAIN =1. It is right?Are my predicted state transition conditions correct?
[A] Yes, that is correct. But do not also forget about the PORB_FS=1 referring to the Fail Safe.
With Best Regards,
Jozef