Hello,
I designed MC33908 circuit according AN4766 to provide power to MPC5744p. When I debug the hardware, there is a strange phenomenon. When I first turn on the 12v switch power supply, then provide power the MC33908, MC33908 did not give its output. But when I truned off the switch power supply and power supply connector still connet to MC33908, then I turned on the power supply again. MC33908 can provide power to MCU and AUX devices. The system works fine. I tried many times, the phenomenon can repeatly appeared. I tested the circuit many times. There is no fault on circuit. Can someone tell me why MC33908 has such a phenomenon? What can I do to improve it?
PS: The debug pin is active.
Hello,
I changed my power supply to a battery. It can not work .
I also changed to a adjustable power supply, when the voltage was between 7~10V, it could work. when voltage was above 10v, it failed.
Thank you. I found where the error hanppened.
I add a 100nF capacity in buck circuit with diode D1, then pin VSW1 VSW2 can not generate PWM. After I remove the capacity, it works. But in AN4766, it gives the Vpre characteristics, the FSWPRE is 440 kHz, I check the frequency is about 300 kHz. Is it OK? Are there some risks when I use it ?