Hello NXP,
wanted to update the DPDK from 21.11 to 22.11 on below source
1.repo init -u https://github.com/nxp-qoriq/yocto-sdk.git -b kirkstone -m ls-5.15.71-2.2.0_distro.xml
could you please help the steps to modify the same
thanks,
ranga
you can try following options : Change the dpdk-commit and URL in meta layer:
/opt/lldp/sources/meta-qoriq/recipes-extended/dpdk/dpdk-21.11.inc
SRC_URI = "git://github.com/nxp-qoriq/dpdk;protocol=https;nobranch=1"
SRCREV = "40adc5753bc624c469459ab5261ae36109dbe7eb"
Or, in your meta layer, you can write a dpdk*.bbappend file to overwrite the dpdk repo Path and commit.
Hello NXP,
Also i dont want to move to new source as GCC ,binutils version will get upgraded , Any method to update DPDK 22.11 on the below source itself
repo init -u https://github.com/nxp-qoriq/yocto-sdk -b mickledore -m ls-6.1.55_2.2.0_distro.xml
Hello,
DPDK 22.11 is supported on below source:
repo init -u https://github.com/nxp-qoriq/yocto-sdk -b mickledore -m ls-6.1.55_2.2.0_distro.xml
Have a nice day!!
Hello Team,
I am getting the below error:
python3 repo init -u https://github.com/nxp-qoriq/yocto-sdk -b mickledore -m ls-6.1.55_2.2.0_distro.xml
repo: reusing existing repo client checkout in /FSM20056_DPDK22
fatal: manifest 'ls-6.1.55_2.2.0_distro.xml' not available
fatal: manifest ls-6.1.55_2.2.0_distro.xml not found
Hello,
In the LLDP, DPDK v22.11 is supported under Kernel v6.1.55, that's why you have to download the poky repository and bitbake tools using the repo tool in a new project.(build and bitbake again from the beginning).