When trying to execute the GUI of PF3000 programming, I'm getting message "Referência de objeto não definida para uma instância de um objeto." = Object's reference not defined for an objects' instance.
Also the kit KITPF3000FRDMPGM seems not to be running, because no device is detected on win10 USB ports.
Is available the firmware of KITPF3000FRDMPGM, so I could try to reflash it ?
Thanks
Hi Sun,
How to do it ? This is my first community access, I didn't know of tickets.
This page suggested me another questin related to PF3000, and it looks like the same problem I'm having :
( Question by Max Liu in 14/06/2017 ; Last answer in 15/06/2017 by Kan_Li ).
Also the RGB leds from KSZ25 board are changing colors, it seems to me when the board was ok, the leds were not this way.