JN5189

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

JN5189

613 次查看
qianchihuang
Contributor III

I compiled and generated a EndDerive_OM15082.axf and I wanted to debug it through Debug, but he reported the following error。

qianchihuang_1-1688992793176.png

qianchihuang_2-1688993358738.png

How do I adjust it so that he can generate JN-AN-1243-Zigbee-3-0-Base-Device.axf?

 

0 项奖励
回复
2 回复数

583 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. In order to debug the AN, you would need to follow these steps:

Enable the DEBUG in the Makefile:

Ricardo_Zamora_0-1689119051134.png

 

The MCU Settings must select the JN5189 device and the linker server JN5189_640K.cfx

Ricardo_Zamora_1-1689119051135.png

 

Also, you will need to change the root of the axf file. You have to select the example that you previously compiled:

Ricardo_Zamora_2-1689119051137.png

 

Hope this helps.

 

Regards,

Ricardo

0 项奖励
回复

567 次查看
qianchihuang
Contributor III

Hello,Ricardo.

Using the method you provided, I have successfully launched the debugging interface, but it shows No source available for "main() at 0x7086".

qianchihuang_0-1689129809533.png

In addition, I want to see the stack status of 1243, and it is not displayed, so how can I see the stack.

qianchihuang_1-1689129943853.png

Regards,

qianchihuang

 

0 项奖励
回复