Interfacing with System Basis Chip ( SBC ) = MC33905S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing with System Basis Chip ( SBC ) = MC33905S

Jump to solution
1,725 Views
NewbieMCULover
Contributor II

Hi!

I am having problems interfacing with the MC33905S. I am able to send and read SPI data to/from the MC33905S however, the circuit is always on Debug mode (wired the DBG pin to a 9V source, so that it will not reset during programming of MCU)... Sending an SPI command to release it from debug mode does nothing... As I had been checking the response, it is still on debug mode. I had checked the datasheet and it left me clueless for now...

Anybody who have some sample snippets of the flow of initialization? I just need to enable LIN and CAN transceivers from debug mode... Thanks

0 Kudos
Reply
1 Solution
805 Views
NewbieMCULover
Contributor II

Please disregard this, I was able to solve this...

View solution in original post

0 Kudos
Reply
1 Reply
806 Views
NewbieMCULover
Contributor II

Please disregard this, I was able to solve this...

0 Kudos
Reply