Hello,
I have a IMX8QXP-MEK board.
I wanted to use LPUART3, so I added the following lines in the DTS:
&iomuxc {
(...)
pinctrl_lpuart3: lpuart3grp {
fsl,pins = <
IMX8QXP_FLEXCAN2_TX_ADMA_UART3_TX 0x06000020
IMX8QXP_FLEXCAN2_RX_ADMA_UART3_RX 0x06000020
>;
};
(...)
}
But I had this error message when I booted it:
imx8qxp-pinctrl scu:pinctrl: pin_config_set op failed for pin 110 3a83d088 2
(with pin 110 = IMX8QXP_FLEXCAN2_TX)
I discovered I could not configure IMX8QXP_FLEXCAN2_TX, IMX8QXP_FLEXCAN2_RX.
When I do "cat /sys/kernel/debug/pinctrl/scu:pinctrl/pinconf-pins":
(...)
pin 109 (IMX8QXP_FLEXCAN2_RX): N/A
pin 110 (IMX8QXP_FLEXCAN2_TX): N/A
pin 111 (IMX8QXP_UART0_RX): 0x6000020
pin 112 (IMX8QXP_UART0_TX): 0x6000020
pin 113 (IMX8QXP_UART2_TX): 0x6000020
pin 114 (IMX8QXP_UART2_RX): 0x6000020
(...)
IMX8QXP_FLEXCAN2 are seen N/A.
Other pins are N/A (ex : IMX8QXP_QSPI0A, IMX8QXP_QSPI0B...) and they cannot be configure neither.
If I tried to follow what is going wrong in the code: when the code tries to configure the pin in calling SCU with imx_scu_ipc_write(), it returns IMX_SC_ERR_NOACCESS.
Even in the u-boot program, I cannot configure these pins: when I tried to read these pins with sc_pad_get(), I have the error -13, access problem.
So it seems SCU locks this access but why?
Is there a configuration file?
Can SCFW be responsible? Or any other software running before u-boot?
If you have any idea, it is welcome!!
解決済! 解決策の投稿を見る。
Hi Philippe
one can look at similar issue on
Best regards
igor
Thank you Igor, it solves my problem.
Hi Philippe
one can look at similar issue on
Best regards
igor