IMX31_PDK14_LINUX_BSP_R14 Demo images are not booting.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX31_PDK14_LINUX_BSP_R14 Demo images are not booting.

1,788件の閲覧回数
Ramesh_Danlaw
Contributor I

I have imx31 3 stack board. It came with the demo linux. It is working properly. Recently i downloaded the IMX31_PDK14_LINUX_BSP_R14 Demo images from the free scale . I am not able to boot this image. Where as i am able to boot with the old demo images?

Could any one helps me on this?

I am using PDK1.2.

Is there any issue with the hardware version ?

are these IMX31_PDK14_LINUX_BSP_R14 demo images can be run on PDK1.2?

 

Thank you,

S.Ramesh Chandra.

0 件の賞賛
返信
3 返答(返信)

718件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
Please use number 1.
 
Regards,
 
Fabio Estevam
0 件の賞賛
返信

718件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee
Dear S.Ramesh,
 
Have you upgraded your Redboot version? You can't use the bootloader from SDK1.2 on SDK1.4. I suggest you that you do a full erase in your board (using ATK tool), then flash the bootloader that comes with SDK1.4 and try again.
 
Regards,
 
Fabio Estevam
0 件の賞賛
返信

718件の閲覧回数
Ramesh_Danlaw
Contributor I
 
Hi Fabio Estevam,
 
  Thanks for your response
  I found two redboot images listed below  with the demo images i downloaded? Which one i have to download?
 
1. mx31_3stack_redboot
2.mx31_3stack_redboot_mmc
 
Regds,
S.Ramesh Chandra.
 
0 件の賞賛
返信