Hi everyone,
I’m considering upgrading my development setup and am curious about the performance of NXP's IDE on different types of laptops. Specifically, I’m looking into using a 2-in-1 laptop for my NXP development work and would like to know how it stacks up against traditional laptops in this context.
Here are some specifics about my situation:
NXP IDE Version: v 11.8.1
2-in-1 Laptop Model: Yoga 7 2-in-1 (14", Gen 9) AMD
Traditional Laptop Model: oga
Processor & RAM Specifications for Both Laptops:
AMD Ryzen™ 5 8640HS Processor * GB ram 512 SSD
Window 11
I’m particularly interested in:
Performance Comparison: How does the performance of NXP’s IDE on a 2-in-1 laptop compare to a traditional laptop? Are there noticeable differences in speed, responsiveness, or stability?
Usability and Experience: How does using a 2-in-1 laptop affect your development workflow with NXP tools? Are there any usability issues or advantages?
System Requirements: Are there specific hardware or software configurations needed to optimize NXP’s IDE on a 2-in-1 laptop?
Recommendations: If you’ve used NXP’s IDE on both types of laptops, which do you prefer and why? Are there particular 2-in-1 models that perform better for this purpose?
I appreciate any insights or personal experiences you can share. Thanks in advance for your help!
Hi @Daniellemorriss,
MCUXpresso IDE does not really benefit from the use of a 2-in-1 over a conventional one, as it is not designed with extra features for these kinds of laptops. As long as the IDE runs on a laptop that complies with the specifications shown on the Instalation Guide, the performance should be OK, regardless of whether it's running on a conventional or a 2-in-1 laptop.
BR,
Edwin.