How to support CAN FD in CanTrcv?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to support CAN FD in CanTrcv?

1,357件の閲覧回数
nourhankhedr
Contributor I

Hello All,

I need to confirm my understanding to "TJA1145 Datasheet". Is it mandatory to have PN enabled/configured in order to support CAN FD in CanTrcv? Also, I would like to ask what is the necessary changes needed on CanTrcv in order to support CAN FD? 

Thanks in advance

タグ(1)
0 件の賞賛
返信
4 返答(返信)

812件の閲覧回数
nxp_jeremyzhou
Contributor I
 
0 件の賞賛
返信

1,196件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

As per datasheet TJA1145 enables reliable communication in the CAN FD fast phase at data rates up to 2 Mbit/s. No configuration is needed.

Moreover the TJA1145 implements so-called FD-passive functionality. It is the ability to ignore CAN FD frames while waiting for a valid wake-up frame in Sleep/Standby mode. This feature of partial networking is useful on networks that support both CAN FD and standard CAN 2.0 communications. It allows normal CAN controllers that do not need to communicate CAN FD messages to remain in partial networking Sleep/Standby mode during CAN FD communication without generating bus errors.

BR, Petr

791件の閲覧回数
nxp_jeremyzhou
Contributor I
Hello, after power on, i read the NMS and MC , NMS is 1(not entered Normal), MC is 100(standby). after i send cmd to let it goes Normal, then i check the MC and NMS, the MC is still 100, but NMS is 0? do you have any ideal?
0 件の賞賛
返信

808件の閲覧回数
nxp_jeremyzhou
Contributor I
the frame control rgister (address 2Fh), DLC only support 8 bytes? if the can FD message is 64 bytes, how it works?
0 件の賞賛
返信