Hello All.
I bought a SJA1105 Application Board to verify AVB strteam between SJA1105 and R-Car so on.
I had tried to set clock synchronization parameters SWMASTER, ETSSRCPCF etc, and made a new configuration file and run test.bat to install the newconfig.hex.
But I could not running gptp on the SJA1105.
Please tell me if something wrong or missing.
Best Regards.
已解决! 转到解答。
There is a drivers package on NXP docstore which offers a few ready
gPTP configurations for the switch under cfg\ directory. Please register
on Docstore, obtain the package and try. The package name is
"sw427402 - Drivers (0.2)".
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
hi Eisuke Tada,
There is the NXP reply,
“For a successful registration a Nondisclosure Agreement – NDA - between your company and NXP is required”
Hi Eisuke Tada
Did you resolve SJA1105 config issue?
Now I can't register Docstore anymore. It says "
Would you like to share the "sw427402 - Drivers (0.2)". to me?
My email is xinting.gu@enjoymove.cn
Thank you.
There is a drivers package on NXP docstore which offers a few ready
gPTP configurations for the switch under cfg\ directory. Please register
on Docstore, obtain the package and try. The package name is
"sw427402 - Drivers (0.2)".
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------