How to run 802.1AS(gptp) on the SJA1105 Application Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run 802.1AS(gptp) on the SJA1105 Application Board

Jump to solution
1,776 Views
eisuke_tada
Contributor I

Hello All.

I bought a SJA1105 Application Board  to verify AVB strteam between SJA1105 and R-Car so on.

I had tried to set clock synchronization parameters SWMASTER, ETSSRCPCF etc, and made a new configuration file and run test.bat to install the newconfig.hex.

But I could not running gptp on the SJA1105.

Please tell me if something wrong or missing.

Best Regards.

Labels (1)
0 Kudos
1 Solution
1,405 Views
bpe
NXP Employee
NXP Employee

There is a drivers package on NXP docstore which offers a few ready
gPTP configurations for the switch under cfg\ directory. Please register
on Docstore, obtain the package and try. The package name is
"sw427402 - Drivers (0.2)".


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
1,405 Views
eisuke_tada
Contributor I

Hello xinting guF.

Unfortunately, I am in the same situation.

Best Regrads,

0 Kudos
1,405 Views
xinting_gu
Contributor II

hi Eisuke Tada

   There is the NXP reply,

    “For a successful registration a Nondisclosure Agreement – NDA -  between your company and NXP is required

0 Kudos
1,405 Views
xinting_gu
Contributor II

Hi Eisuke Tada

    Did you resolve SJA1105 config issue?

    Now I can't  register Docstore anymore. It says "

The registration of new accounts is current not possible."

 Would you like to share the "sw427402 - Drivers (0.2)". to me?

 My email is xinting.gu@enjoymove.cn

 Thank you.

0 Kudos
1,405 Views
eisuke_tada
Contributor I

Hello Platon.

Thank you for replying, I would register Docstore and try the package before long.

Best Regards

0 Kudos
1,406 Views
bpe
NXP Employee
NXP Employee

There is a drivers package on NXP docstore which offers a few ready
gPTP configurations for the switch under cfg\ directory. Please register
on Docstore, obtain the package and try. The package name is
"sw427402 - Drivers (0.2)".


Have a great day,
Platon

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos