How to configure the SPI function for D0 and D18 of JN5169

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to configure the SPI function for D0 and D18 of JN5169

ソリューションへジャンプ
516件の閲覧回数
liyouliu
Contributor II

Dear Sir,

Hello, I want to use the DO0 pin and DIO18 pin to configure them as
SCLK and SPIMOSI function. What should I do?

Thank you.

0 件の賞賛
返信
1 解決策
486件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello.

According to the JN5169 datasheet, when the device reset is active, all the SPI-bus master pins are configured as inputs with their pull-up resistors active. The pins stay in this state until the SPI-bus master block is enabled.

Control of the SPI Master using functions of the integrated API is described in JN516x Integrated Peripherals API User Guide, Chapter 14 Serial Peripheral Interface (SPI) Master. Section 14.5 describes how to use the API functions to operate the SPI.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
487件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello.

According to the JN5169 datasheet, when the device reset is active, all the SPI-bus master pins are configured as inputs with their pull-up resistors active. The pins stay in this state until the SPI-bus master block is enabled.

Control of the SPI Master using functions of the integrated API is described in JN516x Integrated Peripherals API User Guide, Chapter 14 Serial Peripheral Interface (SPI) Master. Section 14.5 describes how to use the API functions to operate the SPI.

Regards,
Eduardo.

0 件の賞賛
返信