Hi,
I am using LS1046ARDB board for one of my project, in that I am able to build the yocto root file system and loaded into board it was booted properly but now my problem is I am unable to load the any of the kernel modules in it so I check the /etc/modules-load.d directory nothing is there in that.
root@DevelLinux:/etc/modules-load.d# ls
root@DevelLinux:/etc/modules-load.d#
Please help me out of this to resolve this problem (or let know how to add the kernel modules on build)
Thanks & Regards,
Chethan GR.
Kernel modules are deployed in bootpartition tar ball, after execute the following command, Kernel modules are deployed in the second partition.
flex-installer -b bootpartition_LS_arm64_lts_5.4.tgz -r
rootfs_lsdk2012_yocto_devel_arm64.tgz -d /dev/sdx
On the target board, Kernel modules are mounted in folder /boot/modules/ automatically after the system booting up as normal.
You also could mount the second partition of the boot device manually as the following.
root@DevelLinux:~# umount /boot
root@DevelLinux:~# mount | grep boot
root@DevelLinux:~# mount /dev/mmcblk0p2 /boot
[ 1593.148987] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
root@DevelLinux:~# ls /boot/modules/5.10.35/
build modules.builtin modules.dep modules.softdep
kernel/ modules.builtin.alias.bin modules.dep.bin modules.symbols
modules.alias modules.builtin.bin modules.devname modules.symbols.bin
modules.alias.bin modules.builtin.modinfo modules.order source
In addition, you could generate bootpartition tar ball with the following command.
$ flex-builder -i mkbootpartition
Hi,
No, actually there was version problem in that my kernel version and yocto build kernel version
(my kernel version is 4.19.90 and yocto kernel version is 5.12)
so Please let me know the where I can change the version while build the my yocto root file system
Thanks & Regards
Chethan GR
Please generate bootpartition_LS_arm64_lts_4.19.tgz with the following commands.
$ flex-builder -c linux:linux:LSDK-20.12-V4.19 -a arm64
$ flex-builder -i mkbootpartition
First please generate bootpartition_LS_arm64_lts_4.19.tgz with the following command, Kernel modules are deployed in this package.
$ flex-builder -c linux:linux:LSDK-20.12-V4.19 -a arm64
$ flex-builder -i mkbootpartition
Then refer to my first post to deploy bootpartition tar ball and rootfs tar ball to the target board.
After boot up Linux OS, please mount the second partition to /boot folder to get Kernel modules.
root@DevelLinux:~# mount /dev/mmcblk0p2 /boot
[ 1593.148987] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
root@DevelLinux:~# ls /boot/modules/5.10.35/
Hi,
-> I gave the command to build Linux using "$ flex-builder -c linux:linux:LSDK-20.12-V4.19 -a arm64"
-> Then build the boot tar ball using "$ flex-builder -i mkbootpartition"
Loaded into target machine
root@DevelLinux:~# ls /boot/modules/4.19.139/
extra/ modules.alias modules.builtin modules.dep modules.devname modules.softdep modules.symbols.bin
kernel/ modules.alias.bin modules.builtin.bin modules.dep.bin modules.order modules.symbols
But kernel modules are not loaded on boot-up time
Thanks & Regards,
Chethan GR
Please mount the second partition manually with the following command.
# mount /dev/mmcblk0p2 /boot
Hi,
Below is output of manually I mounted the partition 2,
root@DevelLinux:~# mount /dev/mmcblk0p2 /boot
[ 60.546056] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
root@DevelLinux:~# lsmod
Module Size Used by
root@DevelLinux:~#
Thanks & Regards,
Chethan GR.
Kernel modules cannot be inserted automatically during the system booting up, you need to insert required Kernel modules manually.