Field application problems of TJA1040T/CM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Field application problems of TJA1040T/CM

311 次查看
SwayZhou666
Contributor I

Dear,

My customer is failed to communicate with end customer. But they can normal communication on thier own board. Only 0.1V of CANH & CANL, that we finally find that they have input 5V to 5P(SPLIT PIN, common-mode stabilization output), and suggest them to connect as below:

SwayZhou666_0-1705561234649.png

 

 

SwayZhou666_1-1705561234667.png

Although we have confirmed the problem, my customer still hope we can explain why CANH &CANL’s output only 0.1V but still can communicate.

Pls help to explain.Many thx!

0 项奖励
回复
1 回复

297 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Dear Sway,

I do not fully understand your question, but yes, the SPLIT pin is an output pin to stabilize a common mode point by offering a voltage source of nominal VCC/2. It should be used if there are un-powered nodes while other nodes keep communicating. The DC stabilization aims to oppose this degradation and helps improving the emission performance.

Best regards,

Tomas

0 项奖励
回复