Establish communication with OneWire probe DS18B20 using IO of PCA9574

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Establish communication with OneWire probe DS18B20 using IO of PCA9574

627 Views
dhineshpitchai
Contributor II

Hi team,

In our STM32L082 based board we use PCA9574, as we do not have enough pins in the micro-controller.

We have to use one of the IO pin of PCA9574 to establish communication with One Wire probe DS18B20.

I am facing challenges in establishing communication, as the default Arduino based One Wire library will not be helpful and I have developed similar library to use PCA9574 IO pin.

But that does not help in establishing communication.

Can anyone please help me with this issue.

- Dhinesh

Tags (3)
0 Kudos
Reply
3 Replies

422 Views
dhineshpitchai
Contributor II

Thank you for quick reply, due to time constraints with one-wire protocol using IO of an IO expander as data line will not work

0 Kudos
Reply

602 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

I am afraid that the PCA9574 device does not feature the one-wire interface. I know that it is a similar concept of the I2C but, unfortunately, we do not have any experience with it.

The device might work but it is not guaranteed. 

0 Kudos
Reply

422 Views
dhineshpitchai
Contributor II
 
0 Kudos
Reply