Does DSPD56371AF180 processor include all features of DSPB56371AF180? That is, DSPD56371 has Generic, mini-SA and PPP as its base line in its software code? Related NXP document is: DSPDECODERMSC.pdf (nxp.com). Is there somewhere where the difference between these two part numbers is summarized? ('D' vs. 'B')
Hi,
The DSPB56371AF180 includes the basic Generic, mini-SA and PPP, but does not includes the decoder code in ROM.
The DSPD56371AF180 includes the basic Generic, mini-SA and PPP, and includes the decoder code such as AC-3....
Pls download DSPA56371.pdf from the link:
https://www.nxp.com.cn/docs/en/user-guide/DSPA56371SUM.pdf
But I have not DSPD56371SUM.pdf.
Because the DSP56300 has been end of life, we have not resource to support the audio feature.
Hope it can help you
BR
XiangJun Rong
Thanks XiangJun Rong. Follow-up questions on this if you don't mind?
I greatly appreciate your assistance with this!
Best regards,
Craig Stiegman
Avnet FAE
Hi,
As the following picture, DSPA56371 and DSPB56371 and DSPD56371 are pin to pin compatible, the only different is the ROM code and data.
For the DSPA56371AF150, you have to run it in 150MHz at most, For the DSPA56371AF180, you can run it in 180MHz at most, exceeding frequency is not recommended.
The temperature range of all of DSP56371 is from 0 to 70 degree.
The DSPD56371AF150 is not ROM blank, it has DD/DTS 5.1 decoding + Dolby Headphone & Dolby Virtual Speaker in ROM
Hope it can help you
BR
XiangJun Rong